I.MX6Q PCM Bluetooth?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6Q PCM Bluetooth?

Jump to solution
2,532 Views
ct3paul
Contributor II

Hi all!

Now,I want to use bluetooth on I.MX6Q_SABRESD.

My BSP is linux-3.0.35.

Is there pcm BT functions on imx6?

Thaks a lot !

Chen

0 Kudos
Reply
1 Solution
2,152 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
2 Replies
2,153 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
2,152 Views
art
NXP Employee
NXP Employee

The i.MX6Q processor itself does not contain any specific Bluetooth-related functions. However, it contains a number of digital audio interfaces (SSI, ESAI) that can handle an external PCM audio devices. The Linux 3.0.35 BSP contains the Bluetooth driver that can handle A2DP and AVRCP profiles. For more information, please refer to the Chapter 41 of the i.MX 6Dual/Quad Linux Reference Manual document, available as the part of the L3.0.35_4.1.0_LINUX_DOCS documentation bundle on the Freescale web site:

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=RDIMX6SABREPLAT&fpsp=1&tab=Documentat...


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply