I.MX6Q Linux Remote Processor Framework OpenAMP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX6Q Linux Remote Processor Framework OpenAMP

2,769件の閲覧回数
Tarek
Senior Contributor I

Hi All,

Is it possible to run the Linux driver "remoteproc" on iMX6Q SabreSD board?

I want Linux to run on cores0,1 and 2 while core 3 is dedicated to an RTOS.

The latest  Freescale kernel linux-imx does provide Remoteproc as a module and a modified Rpmsg.

In chapter 53, in the Linux reference manual there is a brief description on  how to use RPmsg for i.MX7 and i.MX6SoloX but nothing about i.MX6Q.

Is there a similar example for i.MX6Q? If not can you please give me some guide to port the existing code from i.MX7 to i.MX6Q?

Thanks,

Tarek

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

1,813件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Tarek

unfortunately AMP is not supported for i.MX6DQ/SDL on official BSPs, one can look at

Boot The i.mx6 dual With Linux+uC/OS-II AMP

http://community.arm.com/message/15766

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信