I.MX6 Sololite LCD_ENABLE define

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6 Sololite LCD_ENABLE define

Jump to solution
2,552 Views
bpmmaster
Contributor II

I.MX6 Sololite :In Reference Manual and datasheet , I can not find the description for " LCD_Enable ".

I don't know if it's the same as " LCD_DRDY" or " LCD_DE", is this the synchronous

control signal with "HSYNC" and "VSYNC"?

not only a On/OFF control?

Because I need converter the parallel  LCD signals to  LVDS  interface, 

0 Kudos
Reply
1 Solution
2,341 Views
Yuri
NXP Employee
NXP Employee

LCD_ENABLE signal enables the data to be shifted to the display. When disabled, the data is invalid

Please look at ENABLE signal on Figure 21-13 (DOTCLK protocol with programmable parameters)
of IMX6SLRM (Rev. 1, 04/2013)

View solution in original post

0 Kudos
Reply
2 Replies
2,342 Views
Yuri
NXP Employee
NXP Employee

LCD_ENABLE signal enables the data to be shifted to the display. When disabled, the data is invalid

Please look at ENABLE signal on Figure 21-13 (DOTCLK protocol with programmable parameters)
of IMX6SLRM (Rev. 1, 04/2013)

0 Kudos
Reply
2,341 Views
bpmmaster
Contributor II

thanks, Mubin.

0 Kudos
Reply