I.MX6 Sololite LCD_ENABLE define

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX6 Sololite LCD_ENABLE define

ソリューションへジャンプ
2,607件の閲覧回数
bpmmaster
Contributor II

I.MX6 Sololite :In Reference Manual and datasheet , I can not find the description for " LCD_Enable ".

I don't know if it's the same as " LCD_DRDY" or " LCD_DE", is this the synchronous

control signal with "HSYNC" and "VSYNC"?

not only a On/OFF control?

Because I need converter the parallel  LCD signals to  LVDS  interface, 

0 件の賞賛
返信
1 解決策
2,396件の閲覧回数
Yuri
NXP Employee
NXP Employee

LCD_ENABLE signal enables the data to be shifted to the display. When disabled, the data is invalid

Please look at ENABLE signal on Figure 21-13 (DOTCLK protocol with programmable parameters)
of IMX6SLRM (Rev. 1, 04/2013)

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,397件の閲覧回数
Yuri
NXP Employee
NXP Employee

LCD_ENABLE signal enables the data to be shifted to the display. When disabled, the data is invalid

Please look at ENABLE signal on Figure 21-13 (DOTCLK protocol with programmable parameters)
of IMX6SLRM (Rev. 1, 04/2013)

0 件の賞賛
返信
2,396件の閲覧回数
bpmmaster
Contributor II

thanks, Mubin.

0 件の賞賛
返信