I.MX6 Boot Mode bits

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6 Boot Mode bits

2,423 Views
rohininarasipur
Contributor II

Hello, I want to set the BOOT_MODE[1:0] to 00 so that boot from fuses mode gets activated. But I can't seem to find a way to program these bits from the reference manual. Are these bits(BOOT_MODE[1:0]) also a part of efuses or they belong to a register? Please help!! Regards, Rohini

0 Kudos
Reply
2 Replies

1,872 Views
b36401
NXP Employee
NXP Employee

Please note that BOOT_MODE[1:0] are external pins of the processor.

You can pull-up or pull-down them to "program" these bits in hardware.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,872 Views
jan_spurek
NXP Employee
NXP Employee

Hi,

BOOT_MODE[1:0] can be accessed via BOOT_MODE0 and BOOT_MODE1 pins.

0 Kudos
Reply