关于imx6dl cpu 在关机充电态下不能显示图片的问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

关于imx6dl cpu 在关机充电态下不能显示图片的问题

936 Views
ninglu
Contributor II

你好:

我们现在相同的主板分别搭载了imx6dl 和imx6d   cpu

在关机充电时,会进入关机充电态,这时候会显示电池图片。

现在imx6d  cpu  在关机充电态时,是会显示电池图片的。

但是imx6dl cpu 在进入关机充电态后,却不能显示图片,屏无任何图片显示。但是在uboot、kernel、android下,dl cpu 显示都是正常的。

以下是imx6dl cpu在充电态下的一些日志。

charger:

charger: ************* END LAST KMSG *************

charger:

charger: --------------- STARTING CHARGER MODE ---------------

failed to read font: res=-1

can't open /dev/tty0: No such file or directory

framebuffer: fd 4 (720 x 1280)

以下的则是imx6q的一些日志

No errors detected

charger:

charger: ************* END LAST KMSG *************

charger:

charger: --------------- STARTING CHARGER MODE ---------------

type=1400 audit(86454.500:4): avc:  denied  { entrypoint } for  pid=2279 comm="init" path="/sbin/healthd" dev=rootfs ino=1476 scontext=u:r:healthd:s0 tcontext=u:object_r:rootfs:s0 tclass=file

healthd: wakealarm_init: timerfd_create failed

healthd: BatteryTemperaturePath not found

healthd: BatteryTechnologyPath not found

: No such file or directory

init: cannot expand '${sys.sysctl.extra_free_kbytes}' while writing to '/proc/sys/vm/extra_free_kbytes'

init: property 'persist.sys.usb.config' doesn't exist while expanding '${persist.sys.usb.config}'

init: cannot expand '${persist.sys.usb.config}' while assigning to 'sys.usb.config'

framebuffer: fd 4 (720 x 1280)

Labels (2)
0 Kudos
Reply
1 Reply

816 Views
jimmychan
NXP TechSupport
NXP TechSupport

which bsp are you using?

0 Kudos
Reply