I.MX6. 24M crystal cannot work,

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

I.MX6. 24M crystal cannot work,

跳至解决方案
3,296 次查看
星辰王
Contributor I

Hi ,ALL!

          I need help of I.MX6. my board cannot up because of  24M crystal  canot work,

          I measure pin NVCC_PLL_OUT is 1.1V, but XTALI  keep  low (XTALO can up to 1.1V).

          This is caused by what reason,let me known, thanks a lot.

标签 (1)
0 项奖励
回复
1 解答
2,921 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,922 次查看
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 项奖励
回复
2,921 次查看
Yuri
NXP Employee
NXP Employee

Please check Your design regarding 24 MHz oscillator requirements in
Table 2-7 (Oscillator and clock recommendations) of the Hardware Development
Guide for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families of Applications Processors
(IMX6DQ6SDLHDG).
In particular, please pay attention on the EB830 document.

https://freescale.hosted.jivesoftware.com/docs/DOC-93757

https://freescale.hosted.jivesoftware.com/servlet/JiveServlet/downloadBody/93757-102-4-3688/EB830%20...

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复