I.MX6. 24M crystal cannot work,

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I.MX6. 24M crystal cannot work,

ソリューションへジャンプ
3,355件の閲覧回数
星辰王
Contributor I

Hi ,ALL!

          I need help of I.MX6. my board cannot up because of  24M crystal  canot work,

          I measure pin NVCC_PLL_OUT is 1.1V, but XTALI  keep  low (XTALO can up to 1.1V).

          This is caused by what reason,let me known, thanks a lot.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,980件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,981件の閲覧回数
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 件の賞賛
返信
2,980件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please check Your design regarding 24 MHz oscillator requirements in
Table 2-7 (Oscillator and clock recommendations) of the Hardware Development
Guide for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families of Applications Processors
(IMX6DQ6SDLHDG).
In particular, please pay attention on the EB830 document.

https://freescale.hosted.jivesoftware.com/docs/DOC-93757

https://freescale.hosted.jivesoftware.com/servlet/JiveServlet/downloadBody/93757-102-4-3688/EB830%20...

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信