I.MX6. 24M crystal cannot work,

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I.MX6. 24M crystal cannot work,

Jump to solution
3,356 Views
星辰王
Contributor I

Hi ,ALL!

          I need help of I.MX6. my board cannot up because of  24M crystal  canot work,

          I measure pin NVCC_PLL_OUT is 1.1V, but XTALI  keep  low (XTALO can up to 1.1V).

          This is caused by what reason,let me known, thanks a lot.

Labels (1)
0 Kudos
Reply
1 Solution
2,981 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!

View solution in original post

0 Kudos
Reply
2 Replies
2,982 Views
CommunityBot
Community Manager
This an automatic process.

We are marking this post as solved, due to the either low activity or any reply marked as correct.

If you have additional questions, please create a new post and reference to this closed post.

NXP Community!
0 Kudos
Reply
2,981 Views
Yuri
NXP Employee
NXP Employee

Please check Your design regarding 24 MHz oscillator requirements in
Table 2-7 (Oscillator and clock recommendations) of the Hardware Development
Guide for i.MX 6Quad, 6Dual, 6DualLite, 6Solo Families of Applications Processors
(IMX6DQ6SDLHDG).
In particular, please pay attention on the EB830 document.

https://freescale.hosted.jivesoftware.com/docs/DOC-93757

https://freescale.hosted.jivesoftware.com/servlet/JiveServlet/downloadBody/93757-102-4-3688/EB830%20...

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply