I. MX 8mn ddr3levk yocto project build problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I. MX 8mn ddr3levk yocto project build problem

1,481件の閲覧回数
jack_huang1
Contributor III

Dear:

     I use the ubantu 20.04 virtual machine

     I use the next command to build the imx8mnddr3levk linux L5.10.35.2.0.0

 

$ DISTRO=fsl-imx-xwayland MACHINE=imx8mnddr3levk source imx-setup-release.sh -b imx8mnD3l_l535xwayland

 

$ bitbake imx-image-multimedia

 

At the end of “bitbake imx-image-multimedia”, do-image-wic generate an error, reference this error with the log file “log.do_image_wic.17779”

The log file is attached.

Thank you!

 

 

0 件の賞賛
返信
2 返答(返信)

1,459件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport

Hello Jack.

For better understand this problem, please provide details as followings:

What steps you have taken before the image build?

what the Virtual machine is and its version? 

Best regards

Harvey

0 件の賞賛
返信

1,456件の閲覧回数
jack_huang1
Contributor III

After changing the Ubuntu version 18.04, the problem is resolved.Thank you!