Hypervisor Support for IVI Platforms

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hypervisor Support for IVI Platforms

2,286件の閲覧回数
danielchempolay
Contributor II

Hi all,

    From https://community.nxp.com/message/802347?et=watches.email.thread#comment-802347., it is said that there is no support for Hypervisor in I.mx Platfroms., but QorIQ Platform has Hypervisor support. Our query is whether the QorIQ Processing Platform is powerful enough to load  Android+Linux, so that we can implement solutions like IVI and also meet time critical requirements?

Best Regards,

Daniel

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,032件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Strictly speaking, QorIQ LS2 is very powerful platform, but

we do not have Android support for it.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,032件の閲覧回数
danielchempolay
Contributor II

Thanks Yuri, Could you then suggest me a platform where i can get support for our requirements as said above?

Regards,

Daniel

0 件の賞賛
返信

2,032件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  NXP does not support hypervisor technology for i.MX6 series, but

customers can try using KVM feature of Linux kernel. You may consider

i.MX6 Q Plus.

Regards,

Yuri.

0 件の賞賛
返信