Hypervisor Support for IVI Platforms

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Hypervisor Support for IVI Platforms

2,354 次查看
danielchempolay
Contributor II

Hi all,

    From https://community.nxp.com/message/802347?et=watches.email.thread#comment-802347., it is said that there is no support for Hypervisor in I.mx Platfroms., but QorIQ Platform has Hypervisor support. Our query is whether the QorIQ Processing Platform is powerful enough to load  Android+Linux, so that we can implement solutions like IVI and also meet time critical requirements?

Best Regards,

Daniel

标签 (1)
0 项奖励
回复
3 回复数

2,100 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Strictly speaking, QorIQ LS2 is very powerful platform, but

we do not have Android support for it.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,100 次查看
danielchempolay
Contributor II

Thanks Yuri, Could you then suggest me a platform where i can get support for our requirements as said above?

Regards,

Daniel

0 项奖励
回复

2,100 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  NXP does not support hypervisor technology for i.MX6 series, but

customers can try using KVM feature of Linux kernel. You may consider

i.MX6 Q Plus.

Regards,

Yuri.

0 项奖励
回复