Hwclock for RTC1 gets Clock tick timeout error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Hwclock for RTC1 gets Clock tick timeout error

2,576件の閲覧回数
sneha_mohan
Contributor I

I am working on the IMX 8M plus board with Linux running on it.

While investigating the /dev/rtc entries for  with the pcf85263.c driver, observed the hwclock is not working for /dev/rtc1. RTC1 is an i2c based rtc clock.

I am getting the below clock time tick error

# /sbin/hwclock --verbose --show -f /dev/rtc1
hwclock from util-linux 2.36.2
System Time: 1666881296.325971
Using the rtc interface to the clock.
Last drift adjustment done at 1666881131 seconds after 1969
Last calibration done at 1666881131 seconds after 1969
Hardware clock is on local time
Assuming hardware clock is kept in local time.
Waiting for clock tick...
hwclock: select() to /dev/rtc1 to wait for clock tick timed out
...synchronization failed.

0 件の賞賛
返信
1 返信

2,561件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Please check and debug your RTC1 driver.

0 件の賞賛
返信