Hwclock for RTC1 gets Clock tick timeout error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hwclock for RTC1 gets Clock tick timeout error

2,652 Views
sneha_mohan
Contributor I

I am working on the IMX 8M plus board with Linux running on it.

While investigating the /dev/rtc entries for  with the pcf85263.c driver, observed the hwclock is not working for /dev/rtc1. RTC1 is an i2c based rtc clock.

I am getting the below clock time tick error

# /sbin/hwclock --verbose --show -f /dev/rtc1
hwclock from util-linux 2.36.2
System Time: 1666881296.325971
Using the rtc interface to the clock.
Last drift adjustment done at 1666881131 seconds after 1969
Last calibration done at 1666881131 seconds after 1969
Hardware clock is on local time
Assuming hardware clock is kept in local time.
Waiting for clock tick...
hwclock: select() to /dev/rtc1 to wait for clock tick timed out
...synchronization failed.

0 Kudos
Reply
1 Reply

2,637 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Please check and debug your RTC1 driver.

0 Kudos
Reply