How to work Bluetooth on i.MX6 sabre lite Android 4.0.3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to work Bluetooth on i.MX6 sabre lite Android 4.0.3

2,051 Views
XIEEnming
Contributor I

Hi, All.

I'm trying to do the porting of  Bluetooth on i.MX6 sabre lite Android 4.0.3 Platform.

To use Bluetooth,  is there any configurations and changes and additions needed against i.MX6 Android Package before building image and put them into the SD card?

Thank you very much!!

Best regards

Tags (1)
0 Kudos
Reply
8 Replies

1,630 Views
XIEEnming
Contributor I

I‘ve not got the BT chip, it will be given to me next week.

We can talk then.  :=)

Thank you very much.

0 Kudos
Reply

1,630 Views
daiane_angolini
NXP Employee
NXP Employee

you´re right.

I´ve never worked directly with bluetooth, but let me ask you something.

Did your kernel recognizes your bluetooth device?

0 Kudos
Reply

1,630 Views
XIEEnming
Contributor I

I am not porting WiFi, I do the Bluetooth.

The WiFi is not aviarable also now.

sdio interface

Thank you for your help

0 Kudos
Reply

1,630 Views
daiane_angolini
NXP Employee
NXP Employee

Great. Touchscreen is amazing with this version!

Which will be your WIFI? will it be sdio?

Please, take a look on this link, and let me know if it can help you

http://www.imxdev.org/wiki/index.php?title=IMX53_QSB_enable_WIFI_android

0 Kudos
Reply

1,630 Views
XIEEnming
Contributor I

R13.1   yes.

use git,   from google

yes, now use dd  to  push the five  images :  u-boot.bin,  uImage,  uramdisk.img,  system.img  and  recovery.img

The android works well and the the touchscreen is good too.

Now just want to do the porting of Bluetooth.

Thank you for your kindness.

regards

0 Kudos
Reply

1,630 Views
daiane_angolini
NXP Employee
NXP Employee

I know it's 4.0.3

But where did you found it? What's the release name? Is it R13.1? Are you getting this from Google? Linaro?

Are you able to boot the images you have?

0 Kudos
Reply

1,630 Views
XIEEnming
Contributor I

Android 4.0.3

regards

0 Kudos
Reply

1,630 Views
daiane_angolini
NXP Employee
NXP Employee

I don't know. Which android Package you're working with?

0 Kudos
Reply