Hello all,
I had place the RAM of size 4GB, in u-boot it show properly which is below.
CPU: Freescale i.MX6DL rev1.2 at 792 MHz
CPU: Temperature 52 C
Reset cause: WDOG
Board: MX6-SabreSD
I2C: ready
DRAM: 3.8 GiB
MMC: FSL_SDHC: 0
serial
switch to partitions #0, OK
But in the kernel it not showing full memory.It shows as below.
root@ota-p112-b1:~# cat /proc/meminfo
MemTotal: 1800664 kB
MemFree: 1695892 kB
MemAvailable: 1739712 kB
Buffers: 1584 kB
Cached: 80380 kB
I had changed the dtb file, bootargs == mem = 4080M. But doesnt workout.Please help me in
resolving this issue.
Hi kalyan
what bsp used in the case, please try with nxp official releases on below link
If issue will persist, please attach full log/
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------