How to via MFG tool do security boot on the i.mx7d

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to via MFG tool do security boot on the i.mx7d

Jump to solution
1,807 Views
felixhsu
Contributor III

Hi all

 

Follow the AN4581,

The customer use MFG tool still fail execute security boot, as below is related log.

 

199976_199976.pngpastedImage_1.png

 

local\mfgtool\Profiles\linux\OS Firmware\firmware\u-boot-imx7dsabresd_sd.imx
ModuleID[2] LevelID[1]: HAB type mismatch: 0x332233!!!
ModuleID[2] LevelID[10]: *********MxHidDevice[030096B0] Jump to Ramkernel successfully!**********
ModuleID[2] LevelID[1]: MxHidDevice::Write() Error writing to device 0x79.
ModuleID[2] LevelID[1]: RunPlugIn(): TransData(0x877FBFD4, 0x6BBC8,0x0) failed.

 

Could you provide document for i.mx7D?

Thanks.

Original Attachment has been moved to: csf_u-boot_yocto_mfg_3.10.53.txt.zip

Original Attachment has been moved to: MfgTool.log.zip

Labels (4)
0 Kudos
Reply
1 Solution
1,489 Views
Yuri
NXP Employee
NXP Employee

Hello,


  It is needed also to sign u-boot for mfgtools firmware and sign mfgtool firmware zImage,

if use the MFG with closed i.MX device.

 

  Please create request to get more information.

Support|NXP 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

View solution in original post

0 Kudos
Reply
1 Reply
1,490 Views
Yuri
NXP Employee
NXP Employee

Hello,


  It is needed also to sign u-boot for mfgtools firmware and sign mfgtool firmware zImage,

if use the MFG with closed i.MX device.

 

  Please create request to get more information.

Support|NXP 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 Kudos
Reply