How to via MFG tool do security boot on the i.mx7d

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to via MFG tool do security boot on the i.mx7d

跳至解决方案
1,747 次查看
felixhsu
Contributor III

Hi all

 

Follow the AN4581,

The customer use MFG tool still fail execute security boot, as below is related log.

 

199976_199976.pngpastedImage_1.png

 

local\mfgtool\Profiles\linux\OS Firmware\firmware\u-boot-imx7dsabresd_sd.imx
ModuleID[2] LevelID[1]: HAB type mismatch: 0x332233!!!
ModuleID[2] LevelID[10]: *********MxHidDevice[030096B0] Jump to Ramkernel successfully!**********
ModuleID[2] LevelID[1]: MxHidDevice::Write() Error writing to device 0x79.
ModuleID[2] LevelID[1]: RunPlugIn(): TransData(0x877FBFD4, 0x6BBC8,0x0) failed.

 

Could you provide document for i.mx7D?

Thanks.

Original Attachment has been moved to: csf_u-boot_yocto_mfg_3.10.53.txt.zip

Original Attachment has been moved to: MfgTool.log.zip

标签 (4)
0 项奖励
回复
1 解答
1,429 次查看
Yuri
NXP Employee
NXP Employee

Hello,


  It is needed also to sign u-boot for mfgtools firmware and sign mfgtool firmware zImage,

if use the MFG with closed i.MX device.

 

  Please create request to get more information.

Support|NXP 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,430 次查看
Yuri
NXP Employee
NXP Employee

Hello,


  It is needed also to sign u-boot for mfgtools firmware and sign mfgtool firmware zImage,

if use the MFG with closed i.MX device.

 

  Please create request to get more information.

Support|NXP 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 项奖励
回复