How to use uuu emmc flash *. wic.zst file?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use uuu emmc flash *. wic.zst file?

Jump to solution
5,784 Views
lidongxu
Contributor II

I previously built version L5.10 of Yocto's BSP, which has a mirror file of * wic.bz2, so I used this command to flash.

uuu -b emmc_all imx-boot-imx8mp-ai-robot-sd.bin-flash_evk imx-image-multimedia_imx8mp-ai-robot.wic.bz2

However, when building version L6.1, it generated *. wic.zst. Should I use the same command to flash? Do I need to make some modifications?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
5,744 Views
joanxie
NXP TechSupport
NXP TechSupport

refer to the user guide

The following command decompresses zst file and writes into eMMC:
uuu -b emmc_all <bootloader> <rootfs.wic.zst/*>

View solution in original post

0 Kudos
Reply
4 Replies
5,745 Views
joanxie
NXP TechSupport
NXP TechSupport

refer to the user guide

The following command decompresses zst file and writes into eMMC:
uuu -b emmc_all <bootloader> <rootfs.wic.zst/*>

0 Kudos
Reply
5,742 Views
lidongxu
Contributor II
Thank you very much for your reply!
Does this mean that there is no difference between. wic.bz2 and. wic.zst? For Flash ? Can I understand it this way ?
0 Kudos
Reply
5,735 Views
joanxie
NXP TechSupport
NXP TechSupport

 they are just different zip format, old bsp version uses bz2, current bsp uses zst, if you use the latest uuu tool, which should support them both

0 Kudos
Reply
5,729 Views
lidongxu
Contributor II
Thank you very much for your help!

Best wishes
0 Kudos
Reply