How to use i.MX8MP ISP Driver without i2c

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to use i.MX8MP ISP Driver without i2c

692 Views
JH-LEE
Contributor I

Hello, NXP team

I'm facing difficulties in using an IR camera with the i.MX8MP-EVK board

Since the IR camera doesn't support I2C, I have made modifications to the ov5640 and imx8-isi-cap kernel drivers to receive MIPI input, which was successful.

However, I'm having trouble modifying the basler_camera and ov2775 drivers for using ISP. Please let me know if you need further assistance or specific details related to these driver modifications.

Thanks in advance!

Best regards,

Jihoon Lee

@joanxie 

0 Kudos
Reply
1 Reply

660 Views
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @JH-LEE,

I hope you are doing well.

I suggest to please look into the Display User guide for more details.
https://www.nxp.com/docs/en/user-guide/iMX8MP_CAMERA_DISPLAY_GUIDE.pdf

Furthermore, If one wants to disable the i2c then Please disable the node by writing down status = "disable" in mipi node.
Please refer to the below link as an example.
https://community.nxp.com/t5/i-MX-Processors/IMX8MP-mipi-dsi-config-in-devicetree/m-p/1355073

It will be helpful.

Thanks & Regards,
Sanket Parekh

0 Kudos
Reply