How to use i.MX8MP ISP Driver without i2c

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use i.MX8MP ISP Driver without i2c

694件の閲覧回数
JH-LEE
Contributor I

Hello, NXP team

I'm facing difficulties in using an IR camera with the i.MX8MP-EVK board

Since the IR camera doesn't support I2C, I have made modifications to the ov5640 and imx8-isi-cap kernel drivers to receive MIPI input, which was successful.

However, I'm having trouble modifying the basler_camera and ov2775 drivers for using ISP. Please let me know if you need further assistance or specific details related to these driver modifications.

Thanks in advance!

Best regards,

Jihoon Lee

@joanxie 

0 件の賞賛
返信
1 返信

662件の閲覧回数
Sanket_Parekh
NXP TechSupport
NXP TechSupport

Hello @JH-LEE,

I hope you are doing well.

I suggest to please look into the Display User guide for more details.
https://www.nxp.com/docs/en/user-guide/iMX8MP_CAMERA_DISPLAY_GUIDE.pdf

Furthermore, If one wants to disable the i2c then Please disable the node by writing down status = "disable" in mipi node.
Please refer to the below link as an example.
https://community.nxp.com/t5/i-MX-Processors/IMX8MP-mipi-dsi-config-in-devicetree/m-p/1355073

It will be helpful.

Thanks & Regards,
Sanket Parekh

0 件の賞賛
返信