How to use VPU to encode/decode on imx8qxp (linux)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to use VPU to encode/decode on imx8qxp (linux)

4,441 次查看
wasim_nazir
Contributor II

Hi Guys,

I am currently using imx-L4.14.98_2.3.0 linux yocto build on imx8qxp-B0.

I need to create one application to encode/decode h264.

Is there any user-guide to implement enc-dec on Amphion VPU.

I am following this doc(https://www.nxp.com/docs/en/reference-manual/IMX_VPU_APPLICATION_PROGRAMMING_INTERFACE_LINUX_REFEREN... ), which shows way for programming based on RPC but doesn't seems complete.

I have also found end/dec test applications here(imx-test - i.MX Driver Test Application Software )

Is there any other proper doc or sample code to follow, to implement the same.

Thanks in Advance,

Regards,

Wasim

0 项奖励
回复
4 回复数

4,303 次查看
wasim_nazir
Contributor II

Thanks a lot for your response.

How to make sure it is using hw-codec and not the sw-codec?

Regards,

Wasim

0 项奖励
回复

4,303 次查看
fmonte
Contributor IV

If using HW decoding, in dmesg you will find messages stating that the VPU is opened, the buffers allocated etc.

0 项奖励
回复

4,303 次查看
fmonte
Contributor IV

Hi Wasim,

on 8QM we are using the NXP's gst v4l2decoder to decode H264 frames using the VPU. That's working fine.

The missing part is the display of the decoded Amphion tiled format, that's not included in the gstreamer provided with BSP 4.14.98

Francesco

0 项奖励
回复

4,303 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Wasim

I am afraid such nxp publicly available documentation is not available yet,

one can look at third party resources:

MX8 GSTREAMER - Variscite Wiki 

GStreamer Based Image Signal Processor - IMX8 Pipelines 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复