How to use UUU to burn Image

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use UUU to burn Image

933件の閲覧回数
tgt007
Contributor II

Hi  NXP

 

How to use UUU to burn Image?

It is wrong to use the following command

uuu.exe -b emmc Image

0 件の賞賛
返信
3 返答(返信)

912件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

Please try:  uuu -b emmc_all **.wic

Best Regards
Zhiming

0 件の賞賛
返信

904件の閲覧回数
tgt007
Contributor II
The kernel image needs to be burned separately.
0 件の賞賛
返信

888件の閲覧回数
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

 

There are uuu example scripts in  demo images, you can use it to download kernel.

example_kernel_emmc.uuu

 

uuu_version 1.2.39

# Please Replace below items with actually file names
# @_flash.bin			| boot loader
# @_Image			| kernel image, arm64 is Image, arm32 it is zImage
# @_board.dtb			| board dtb file
# @_initramfs.cpio.gz.uboot	| mfgtool init ramfs
# @_rootfs.tar.zst		| rootfs
# @_uTee.tar			| optee image, put dummy _uTee.tar file here if platform is not MX6/MX7*

# This command will be run when i.MX6/7 i.MX8MM, i.MX8MQ
SDP: boot -f _flash.bin

# This command will be run when ROM support stream mode
# i.MX8QXP, i.MX8QM
SDPS: boot -f _flash.bin

# These commands will be run when use SPL and will be skipped if no spl
# SDPU will be deprecated. please use SDPV instead of SDPU
# {
SDPU: delay 1000
SDPU: write -f _flash.bin -offset 0x57c00
SDPU: jump
# }

# These commands will be run when use SPL and will be skipped if no spl
# if (SPL support SDPV)
# {
SDPV: delay 1000
SDPV: write -f _flash.bin -skipspl
SDPV: jump
# }

# use uboot burn bootloader to eMMC
# becaue difference chip, offset is difference
# you can use kernel to do that for specific boards
FB: ucmd setenv fastboot_dev mmc
FB: ucmd setenv mmcdev ${emmc_dev}
FB: flash bootloader _flash.bin

FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi;

FB: ucmd setenv emmc_cmd mmc partconf ${emmc_dev} ${emmc_ack} 1 0
FB: ucmd if test "${emmc_skip_fb}" != "yes"; then run emmc_cmd; fi
FB: ucmd setenv emmc_cmd mmc bootbus ${emmc_dev} 2 0 1;
FB: ucmd if test "${emmc_skip_fb}" != "yes"; then run emmc_cmd; fi

FB: ucmd setenv fastboot_buffer ${loadaddr}
FB: download -f _Image
FB: ucmd setenv fastboot_buffer ${fdt_addr}
FB: download -f _board.dtb
FB: ucmd setenv fastboot_buffer ${initrd_addr}
FB: download -f _initramfs.cpio.gz.uboot
#FB: ucmd setenv bootargs console=${console},${baudrate} earlycon=${earlycon},${baudrate}
FB: acmd ${kboot} ${loadaddr} ${initrd_addr} ${fdt_addr}

# get mmc dev number from kernel command line
# Wait for emmc
FBK: ucmd while [ ! -e /dev/mmcblk*boot0 ]; do sleep 1; echo "wait for /dev/mmcblk*boot* appear"; done;

# serach emmc device number, if your platform have more than two emmc chip, please echo dev number >/tmp/mmcdev 
FBK: ucmd dev=`ls /dev/mmcblk*boot*`; dev=($dev); dev=${dev[0]}; dev=${dev#/dev/mmcblk}; dev=${dev%boot*}; echo $dev > /tmp/mmcdev;

# dd to clear the possible MBR
FBK: ucmd mmc=`cat /tmp/mmcdev`; dd if=/dev/zero of=/dev/mmcblk${mmc} bs=512 count=1
# create partition
FBK: ucmd mmc=`cat /tmp/mmcdev`; PARTSTR=$'10M,500M,0c\n600M,,83\n'; echo "$PARTSTR" | sfdisk --force /dev/mmcblk${mmc}

FBK: ucmd mmc=`cat /tmp/mmcdev`; dd if=/dev/zero of=/dev/mmcblk${mmc} bs=1k seek=4096 count=1
FBK: ucmd sync
# you can enable below command to write boot partition. but offset is difference at difference platform
#FBK: ucmd mmc=`cat /tmp/mmcdev`; echo 0 > /sys/block/mmcblk${mmc}boot0/force_ro
#FBK: ucp  _flash.bin t:/tmp
#FBK: ucmd mmc=`cat /tmp/mmcdev`; dd if=/tmp/_flash.bin of=/dev/mmc${mmc}boot0 bs=1K seek=32
#FBK: ucmd mmc=`cat /tmp/mmcdev`; echo 1 > /sys/block/mmcblk${mmc}boot0/force_ro
FBK: ucmd mmc=`cat /tmp/mmcdev`; while [ ! -e /dev/mmcblk${mmc}p1 ]; do sleep 1; done
FBK: ucmd mmc=`cat /tmp/mmcdev`; mkfs.vfat /dev/mmcblk${mmc}p1
FBK: ucmd mmc=`cat /tmp/mmcdev`; mkdir -p /mnt/fat
FBK: ucmd mmc=`cat /tmp/mmcdev`; mount -t vfat /dev/mmcblk${mmc}p1 /mnt/fat
FBK: ucp  _Image t:/mnt/fat
FBK: ucp  _board.dtb t:/mnt/fat
FBK: ucp  _uTee.tar t:/tmp/op.tar
FBK: ucmd tar --no-same-owner -xf /tmp/op.tar -C /mnt/fat
FBK: ucmd umount /mnt/fat
FBK: ucmd mmc=`cat /tmp/mmcdev`; mkfs.ext3 -F -E nodiscard /dev/mmcblk${mmc}p2
FBK: ucmd mkdir -p /mnt/ext3
FBK: ucmd mmc=`cat /tmp/mmcdev`; mount /dev/mmcblk${mmc}p2 /mnt/ext3
FBK: acmd export EXTRACT_UNSAFE_SYMLINKS=1; tar --zstd --warning=no-timestamp -x -C /mnt/ext3
FBK: ucp  _rootfs.tar.zst t:-
FBK: Sync
FBK: ucmd umount /mnt/ext3
FBK: DONE




Best Regards
Zhiming

0 件の賞賛
返信