How to use SB_loader to load imx in parallel to multiple devices via USB.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use SB_loader to load imx in parallel to multiple devices via USB.

998件の閲覧回数
idan357
Contributor I

Hello All.

Im trying to use SB_loader.xex when i have 4 mx6 devices connected to usb and i want to load them im parallel.

I there a way to direct the SB_loader to a specific USB ? form my tries i noticed the he only load the first usb he encounter.

I didnt see any flag that i can set to direct it to a specific USB port.

BR,

Idan.

タグ(3)
0 件の賞賛
返信
1 返信

879件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Idan

I am afraid currently this is not supported, probably one can try to

modify application using sources

GitHub - NXPmicro/mfgtools: Freescale/NXP I.MX Chip image deploy tools. 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信