How to use PLL to generate precise clock frequency, with Linux, devicetree?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to use PLL to generate precise clock frequency, with Linux, devicetree?

2,815件の閲覧回数
nrch
Contributor I

Hello, I am creating a camera driver for IMX296 for the i.MX 8 MQ. I am struggling with generating the appropriate clock signal for the image sensor, which is either 37.125, 74.25 or 54 MHz.

I base my devicetree on the ov5640, and the devicetree for the imx296 looks like this:

  imx296_mipi: imx296_mipi@1a {
    compatible = "sony,imx296_mipi";
    reg = <0x1a>;
    status = "okay";

    pinctrl-names = "default";
    pinctrl-0 = <&pinctrl_csi1>;

    clocks = <&clk IMX8MQ_CLK_CLKO1_DIV>;
    clock-names = "csi_mclk";
    assigned-clocks = <&clk IMX8MQ_CLK_CLKO1_SRC>, <&clk IMX8MQ_CLK_CLKO1_DIV>;
    assigned-clock-parents = <&clk IMX8MQ_SYS1_PLL_200M>;
    assigned-clock-rates = <0>, <54000000>;

    csi_id = <0>;

    rst-gpios = <&gpio1 7 GPIO_ACTIVE_LOW>;

    mclk = <54000000>;
    mclk_source = <0>;
    port {
      ov5640_mipi1_ep: endpoint {
        remote-endpoint = <&mipi1_sensor_ep>;
      };
    };
  };

 

I try an ask for 54MHz, but the output become 50MHz which indicates that the clock divider used here is rounded to nearest integer, 4.

Is it possible to increase the accuracy of the PLL here, so that I can get these above mentioned frequencies?

I have tried to change assigned-clock-parents to <&clk IMX8MQ_SYS1_PLL_266M> which should be able to get close enough to 54MHz, dividing by 5, but this results in an error: "clk: failed to reparent clko1_div to sys1_pll_266m: -22".

What can I do to achieve the above mentioned frequencies?

ラベル(2)
0 件の賞賛
返信
1 返信

2,704件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nicolai

I believe only reprogramming properly some pll necessary precise clock

may be produced. One can try this in uboot. As for error: "clk: failed to reparent clko1.."

seems this parent pll is already used by some other clock, so it can not be used.

May be useful to look at linux clock documentation:

https://www.kernel.org/doc/Documentation/clk.txt 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信