Hello! I`m trying to find any information about question: How to use AES-128 hardware decryption (with CAAM) on iMX6. I use Variscite board VAR-SOM-SOLO. I was made bootloader (using SDK) for this board and successfully made it encrypted with HAB technology. It`s load good, without any HAB events. The next my step is make encrypted application (using AES-128 cryptography) and bootloader need to load this application from NAND flash to DDR RAM, quickly decrypt this aplication and start it. I try using software AES-128 algorithm, but it to slow.
So I need any code example (using iMX6 registers) which will show how to decrypt my application with AES-128 hardware CAAM accelerator.
Help me please with this trouble.
Regards.
Hello,
hope the following helps.
https://community.nxp.com/thread/433262
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello! Thanks, but this information is not useful for me, becouse I`m not using linux. My application is a project wich use SDK and some RTOS (not linux). I need an example that uses the CAAM registers to decrypt AES-128. Or documentation about CAAM registers to use AES accelerator module.