How to understand "ECC checks the first 4 Kbytes of boot data from NAND Flash Block-0"?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to understand "ECC checks the first 4 Kbytes of boot data from NAND Flash Block-0"?

1,934件の閲覧回数
王剑翰
Contributor III

In I.MX25RM page 143, it is as below:

The boot ROM code makes use of the duplicate boot code according to the following procedure:

• On device power-on, the boot ROM copies the first 4 Kbytes of boot code from the NAND Flash

to the NFC buffer.

• ECC checks the first 4 Kbytes of boot data from NAND Flash Block-0

— If no ECC errors are detected, the downloaded 4 Kbytes image as well as rest of the image is

copied to application destination pointer location (specified in the HAB header) and secure

boot is performed. The application image length is specified in the image header so the boot

ROM reads this to know how much image data to download.

— If ECC Error is detected in first 4 Kbytes of boot data from Block-0, the boot ROM code copies

the duplicated 4k boot data from the NAND flash block-1.

……

In page 153, it says as below:

NFC automatically generates an ECC code for both main and spare data during NFC data load/read

to/from NAND Flash, and NFC updates ECC in the ECC status Register. NFC performs error detection

and error correction. If the number of ECC errors does not exceed the allowable limit (four for 4-bit ECC,

eight for 8-bit ECC), then NFC corrects those errors.

……

Then, I have a question:

1, Do NFC perform the error correction when ECC checks the first 4 Kbytes of boot data from NAND Flash Block-0?

2, If it detect some ECC errors, but the errors' number does not exceed the allowable limit and NFC corrects those errors, which below procedure will follow?

— If no ECC errors are detected, the downloaded 4 Kbytes image as well as rest of the image is copied to application destination pointer location (specified in the HAB header) and secure boot is performed. The application image length is specified in the image header so the boot ROM reads this to know how much image data to download.

— If ECC Error is detected in first 4 Kbytes of boot data from Block-0, the boot ROM code copies the duplicated 4k boot data from the NAND flash block-1.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,797件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi 王剑翰

1. yes, NFC performs the error correction when reading the first 4 Kbytes of boot data from NAND Flash Block-0

2. If it detects some ECC errors, but errors' number does not exceed the allowable limit, NFC corrects those errors

   and follow boot flow described in RM (as in case when no errors were detected).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,797件の閲覧回数
王剑翰
Contributor III

Thank you for your kindly reply.

My customer  also have a question for this (The MPU is i.MX 257 and the nandflash is  MT29F2G08ABBEAH4):

  They modified the ATK source code so that all the spare area of block0 were writed with 0 during programming operation. They hope it can cheat iMX257 that the Block0 of NAND has been borken, and make it boot from block1. But it failed, the board also boot from block0.

So, they want to ask what else ROM code should be changed specially?

0 件の賞賛
返信

1,797件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

I think you can check signals by oscilloscope and

you will find that iROM after fail with block0, will

access to block1, check nand address signals.

For most confidence you can erase entirely block0.

0 件の賞賛
返信