Hello,
I need to trigger a user define software interrupt from Cortex A35 to Cortex M4 in IMX8 board. Please advice.
Linux 4.14.98 is running in A35.
Best regards,
Praveen
Hi Praveen
for available options one can look at Chapter 10
RPC Protocol, "Interrupts" System Controller Firmware API Reference Guide
included in SCFW Porting Kit
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks Igor for quick response.
Do you mean that I can use sc_irq_enable() to generate the interrupt at A35 and sc_irq_status() to read the IRQ value at M4?
Since SCU APIs are kernel library in Linux; do you have any suggestion on how to use it from user space?
Thanks and regards,
Praveen
I am not sure that it is possible to implement that using SCU APIs,
you can find some examples in SDK_MEK-MIMX8QM
Welcome | MCUXpresso SDK Builder
In any way there are no other options for interaction between cores except SCU APIs.
Best regards
igor
Hi Igor,
As per my understanding, to access kernel library we shall create a driver / procfs / sysfs.
What we wanted to be sure that does NXP provides SCU driver for Linux or any procfs file, which can be used to access SCU APIs?
Is there any example in Linux OS, where application is using SCU APIs?
Best regards,
Praveen
Hi Praveen
please read documentation included in SCFW Porting Kit ,
in particular sc_fw_api.pdf
>Is there any example in Linux OS, where application is using SCU APIs?
ipc.c\main\sc\imx\soc\drivers - linux-imx - i.MX Linux kernel
check also sect.2.2 System Controller Linux Manual in Linux 4.19.35_1.1.0 Documentation
Best regards
igor
Hi Igor,
If LSIO #13 MU is used to interrupt M4 from A35 and visa-versa, then where shall in the BSP and M4 code, the config changes be made? And what those changes will be? Will INTMUXC and INT-Steer (and its mapping to M4-NVIC) also gets impacted?
Best regards,
Praveen
Hello Igor,
Waiting for your response for the above queries.
Further to that I have couple of more query:
2. Why NVIC is only in Cortex M4 and SCU?
Best regards,
Praveen
Hi Praveen
regarding your question for "trigger a user define software interrupt from 
Cortex A35 to Cortex M4 in IMX8" - seems SCFW does not provide such option.
Best regards
igor
Hello Igor,
I agree with you; using SCU APIs may not help in this case.
We are planning to use MU11_A and MU11_B for interrupt generation from A35 to M4. In this approach, we seek your support on what all we shall take care.
Best regards,
Praveen
Hi Praveen,
I am interested in implementing a similar use case where M4 signal A35 cores by issuing a remore interrupt, and the same in opposite direction.
Did you finally experiment it ?
Could you give some feedback ?
Thanks in advance,
Best Regards,
Laurent