How to transfer files between multiple IMX6 devices?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to transfer files between multiple IMX6 devices?

2,041 次查看
prasannaprabhu7
Contributor III

I have 4 imx6 devices in which one device will act as server and other as client, connected in a ring fashion via Ethernet and need to transfer data among each other.Currently I am trying with tftp method. I am able to download files using tftp mechanism given one of pc tftp server is running and running tftp client in all the devices. But I am not aware how to setup a tftp server in Imx6 sabre based board because in my requirement I need to transfer among the devices and not from PC. Did any one worked on setting up tftp server in IMX6 or any similar board or any other mechanism to transfer the files among the subordinate IMX6 via ethernet?

Regards,

Prasanna

标记 (3)
0 项奖励
回复
1 回复

1,505 次查看
jimmychan
NXP TechSupport
NXP TechSupport

You may try to use SSH.  this one may be useful for you.

Best way to transfer files over a LAN between two Linux computers - Super User 

0 项奖励
回复