How to transfer files between multiple IMX6 devices?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to transfer files between multiple IMX6 devices?

2,011件の閲覧回数
prasannaprabhu7
Contributor III

I have 4 imx6 devices in which one device will act as server and other as client, connected in a ring fashion via Ethernet and need to transfer data among each other.Currently I am trying with tftp method. I am able to download files using tftp mechanism given one of pc tftp server is running and running tftp client in all the devices. But I am not aware how to setup a tftp server in Imx6 sabre based board because in my requirement I need to transfer among the devices and not from PC. Did any one worked on setting up tftp server in IMX6 or any similar board or any other mechanism to transfer the files among the subordinate IMX6 via ethernet?

Regards,

Prasanna

ラベル(7)
タグ(3)
0 件の賞賛
返信
1 返信

1,475件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

You may try to use SSH.  this one may be useful for you.

Best way to transfer files over a LAN between two Linux computers - Super User 

0 件の賞賛
返信