How to support sgtl5000 with X86 platform

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to support sgtl5000 with X86 platform

1,536 Views
bakbad
Contributor III

Hello, NXP

I had a custom board with x86 cpu and sgtl5000 , and now I need to port sgtl5000 to x86 platform.

Q1: Does sgtl5000 codec support for x86 platform?

Q2: if Q1's answer is yes, how to start with porting sgtl5000 for x86? any advice?

Best Regards,

bo xu.

Labels (3)
0 Kudos
Reply
2 Replies

1,446 Views
jamesbone
NXP TechSupport
NXP TechSupport

Q1.- Not directly, since the SGTL500 requires and I2C port to configure the device and I2S to send the digital AUDIO, nevertheless, we can said it is support by HW, but NXP does not have any driver to offer in the SW side. You can use for starting the porting the Linux Driver Available for our ARM devices, like the available in the following GIT Hub

linux-imx6/imx6qdl-nit6xlite.dtsi at boundary-imx_4.1.15_1.0.0_ga · boundarydevices/linux-imx6 · Git... 

I can strongly suggest that you use another CODEC, since NXP does not recommend this device for new designs.

Hope this clarifies your inquires.

Have a nice day,

TIC Support Team

0 Kudos
Reply

1,446 Views
bakbad
Contributor III

Well,I see. Thank you very much for your answer.

Regards,

bo xu.

0 Kudos
Reply