How to stream video from iMX8M plus using Gstreamer and RTSP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to stream video from iMX8M plus using Gstreamer and RTSP

1,616 Views
Vijay_hegde
Contributor II

I am trying to stream video from my i.MX8M plus board using Gstreamer and RTSP (mediamtx tool).
Trying with gst-launch-1.0 commad (but not has x264enc support) .
Is it only possible using gst-variable-rtsp-server command?

Or can you help me with setting up the things.

 

i.MX8M 

0 Kudos
Reply
5 Replies

1,485 Views
Vijay_hegde
Contributor II

hey can you help me with the system configuration to build imx-image-full. Currently I am doing it on 64 GB RAM and 2TB storage. But process gets killed like system crash.

 

0 Kudos
Reply

1,470 Views
joanxie
NXP TechSupport
NXP TechSupport

pls create a new thread for this new issue, and attach detailed logfile you get(what kind of crash you get), building issue or booting up issue? it's better if you can give us the detailed steps, we can double check it, it's hard to help you if you only said system crash

0 Kudos
Reply

1,565 Views
Vijay_hegde
Contributor II

Thank you.

To use OpenCV and ML do I need imx-full-image or I can build it no top of other image.

 

0 Kudos
Reply

1,559 Views
joanxie
NXP TechSupport
NXP TechSupport

yes, if you want to use ML, you need build full images

joanxie_0-1741951433464.png

 

1,583 Views
joanxie
NXP TechSupport
NXP TechSupport

pls refer to the link as below, the command was tested official before in this link

https://community.nxp.com/t5/i-MX-Processors/Unable-to-get-RSTP-streaming-working-imx8mp/td-p/205146...