How to set the fdt_file value on yocto project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to set the fdt_file value on yocto project

1,602件の閲覧回数
ChChang
Contributor II

Hi

My platform is i.mx8qm-mek, and the BSP is Linux L6.1.55_2.2.0.
Currently, the generated image file uses
imx8qm-mek-rpmsg.dtb as the fdt_file for uboot.
I would like to change the default value of
fdt_file to imx8qm-mek-hdmi.dtb before Yocto generates the image, without manually setting it in uboot.
Which conf file should I modify?
Thanks!

CH

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,556件の閲覧回数
Harvey021
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信

1,552件の閲覧回数
ChChang
Contributor II

Thanks for your reply ,
This problem was solved, thanks a lot!

Regards,

CH

0 件の賞賛
返信