[iMX93AUTO EVK] SPI Configuration for QCA7006AQ with imx93AUTO EVK is not working

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

[iMX93AUTO EVK] SPI Configuration for QCA7006AQ with imx93AUTO EVK is not working

809 次查看
rohitcs0089
Contributor I

Hi Team,

I am working on iMX93 Auto EVK and enabling the communication between iMX93 and QCA7006AQ vi SPI. I am connecting QCA chip on lpspi3 and did following device tree changes in imx93-14x14-evk.dts -

&lpspi3 {
fsl,spi-num-chipselects = <1>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_lpspi3>;
cs-gpios = <&gpio2 8 GPIO_ACTIVE_LOW>;
status = "okay";

qca7006aq: ethernet@0 {
compatible = "qca,qca7006aq";
reg = <0x0>;
interrupt-parent = <&gpio2>; /* GPIO Bank 2 */
interrupts = <17 IRQ_TYPE_LEVEL_HIGH>; /* Index: 17, level triggered */
spi-cpha; /* SPI mode: CPHA=1 */
spi-cpol; /* SPI mode: CPOL=1 */
spi-max-frequency = <14000000>; /* freq: 14 MHz */
local-mac-address = [ A0 B0 C0 D0 E0 F0 ];
};
};

pinctrl_lpspi3: lpspi3grp {
fsl,pins = <
MX93_PAD_GPIO_IO08__GPIO2_IO08 0x31e /* Chip Select */
MX93_PAD_GPIO_IO09__LPSPI3_SIN 0x3fe
MX93_PAD_GPIO_IO10__LPSPI3_SOUT 0x3fe
MX93_PAD_GPIO_IO11__LPSPI3_SCK 0x3fe
MX93_PAD_GPIO_IO17__GPIO2_IO17 0x31e  /* Interrupt*/
>;
};

I am sending command 0xDA00 to read the signature register value but not getting any response on MISO line.

rohitcs0089_0-1711615201371.png

 

we have followed the below link to come out with above mentioned DTS Configuration 

https://coral.googlesource.com/linux-imx/+/refs/heads/codeaurora-linux-4.19.y/Documentation/devicetr...

Please help us to understand what we are missed to configure. 

 

标记 (4)
0 项奖励
回复
2 回复数

716 次查看
qiang_li-mpu_se
NXP Employee
NXP Employee

Hi @rohitcs0089 

From the qca driver function qcaspi_read_register() "https://github.com/qca/qca7000/blob/master/qca-spi/qca_7k.c"  

It seems there is no special requirement for CS signal, it used two transfers to read the register, between two transfer, the CS pin will be pulled to invalid. So I think both "MX93_PAD_GPIO_IO08__GPIO2_IO08" and "MX93_PAD_GPIO_IO08__LPSPI3_PCS0" can work for the qca device.

0 项奖励
回复

777 次查看
Richard_Kim
NXP Employee
NXP Employee

Hi @rohitcs0089,

 

The MISO signal should be generated by slave and it is QCA7006AQ in your design.

You need to ask Qualcomm.

 

Best Regards,

Richard

0 项奖励
回复