How to set the desired DDR frequency using the i.MX8QXP/DXP/DX DDR Register Programming Aid

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to set the desired DDR frequency using the i.MX8QXP/DXP/DX DDR Register Programming Aid

ソリューションへジャンプ
2,429件の閲覧回数
changshui
Contributor I

Hi expert

I have a question about DDR frequency setting. my hardware platform:

    SOC: imx8dx

    DDR: MT53D512M16D1DS

   (DDR model is consistent with the DDR Register Programming Aid)

When I used i.MX8QXP/DXP/DX DDR Register Programming Aid to set the DDR frequency, I found that clock cycle freq only 800M and 1200M could be selected in excel.

DDR_Freq.png

If I want to set the DDR frequency to 1100M, force off cell input validation and set the clock to 1100, is that OK?If not, how to set it

ラベル(1)
0 件の賞賛
返信
1 解決策
2,355件の閲覧回数
pengyong_zhang
NXP Employee
NXP Employee

Hi @changshui 

Because in our default BSP code, the board's DDR default start frequency is the same as the default in the RPA table, we cannot set all the frequency points in our RPA table. There are so many frequency point.

B.R

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,356件の閲覧回数
pengyong_zhang
NXP Employee
NXP Employee

Hi @changshui 

Because in our default BSP code, the board's DDR default start frequency is the same as the default in the RPA table, we cannot set all the frequency points in our RPA table. There are so many frequency point.

B.R

0 件の賞賛
返信
2,341件の閲覧回数
changshui
Contributor I
OK, I konw! Thanks for your help
0 件の賞賛
返信
2,411件の閲覧回数
pengyong_zhang
NXP Employee
NXP Employee

Hi, @changshui 

You can input the DDR frequency point.

B.R

0 件の賞賛
返信
2,388件の閲覧回数
changshui
Contributor I

Hi pengyong

I still have a question. As you described, if I can enter any frequency point, why can excel only select 800M and 1200M frequencies now

B.R

0 件の賞賛
返信