How to set the desired DDR frequency using the i.MX8QXP/DXP/DX DDR Register Programming Aid

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to set the desired DDR frequency using the i.MX8QXP/DXP/DX DDR Register Programming Aid

Jump to solution
2,428 Views
changshui
Contributor I

Hi expert

I have a question about DDR frequency setting. my hardware platform:

    SOC: imx8dx

    DDR: MT53D512M16D1DS

   (DDR model is consistent with the DDR Register Programming Aid)

When I used i.MX8QXP/DXP/DX DDR Register Programming Aid to set the DDR frequency, I found that clock cycle freq only 800M and 1200M could be selected in excel.

DDR_Freq.png

If I want to set the DDR frequency to 1100M, force off cell input validation and set the clock to 1100, is that OK?If not, how to set it

0 Kudos
Reply
1 Solution
2,354 Views
pengyong_zhang
NXP Employee
NXP Employee

Hi @changshui 

Because in our default BSP code, the board's DDR default start frequency is the same as the default in the RPA table, we cannot set all the frequency points in our RPA table. There are so many frequency point.

B.R

View solution in original post

0 Kudos
Reply
4 Replies
2,355 Views
pengyong_zhang
NXP Employee
NXP Employee

Hi @changshui 

Because in our default BSP code, the board's DDR default start frequency is the same as the default in the RPA table, we cannot set all the frequency points in our RPA table. There are so many frequency point.

B.R

0 Kudos
Reply
2,340 Views
changshui
Contributor I
OK, I konw! Thanks for your help
0 Kudos
Reply
2,410 Views
pengyong_zhang
NXP Employee
NXP Employee

Hi, @changshui 

You can input the DDR frequency point.

B.R

0 Kudos
Reply
2,387 Views
changshui
Contributor I

Hi pengyong

I still have a question. As you described, if I can enter any frequency point, why can excel only select 800M and 1200M frequencies now

B.R

0 Kudos
Reply