How to set display contrast or gamma Freescale_Yocto_Project

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to set display contrast or gamma Freescale_Yocto_Project

1,979 次查看
arkceajin
Contributor I

OS: Poky ( Yocto Project Reference Distro ) 1.6.2

Board:  i MAX6Q
I am trying to adjust the display contrast  by this command:

xrandr --output output_name --gamma 1:1:1

Result as fellow:

Desktop Ubuntu : work fine
Yocto : not work

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

1,382 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Hello Ark,

BSPs older than the 3.10.17-1.0.0 release do not support xrandr. I would recommend migrating to the newest BSP possible.

These newer BSP releases do include some documentation regarding the use of the Xserver video driver so you may want to review this documentation as well.

0 项奖励
回复

1,382 次查看
arkceajin
Contributor I

Hello

Thanks for your answer.

the BSP version is imx-3.10.53-1.1.0_ga, and other xrandr command has properly worked, like size,only except xrandr gamma, typed the command into console and nothing happened.

0 项奖励
回复