How to set display contrast or gamma Freescale_Yocto_Project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to set display contrast or gamma Freescale_Yocto_Project

1,980 Views
arkceajin
Contributor I

OS: Poky ( Yocto Project Reference Distro ) 1.6.2

Board:  i MAX6Q
I am trying to adjust the display contrast  by this command:

xrandr --output output_name --gamma 1:1:1

Result as fellow:

Desktop Ubuntu : work fine
Yocto : not work

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,383 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Ark,

BSPs older than the 3.10.17-1.0.0 release do not support xrandr. I would recommend migrating to the newest BSP possible.

These newer BSP releases do include some documentation regarding the use of the Xserver video driver so you may want to review this documentation as well.

0 Kudos
Reply

1,383 Views
arkceajin
Contributor I

Hello

Thanks for your answer.

the BSP version is imx-3.10.53-1.1.0_ga, and other xrandr command has properly worked, like size,only except xrandr gamma, typed the command into console and nothing happened.

0 Kudos
Reply