How to run x application automatically in Wayland environment

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to run x application automatically in Wayland environment

ソリューションへジャンプ
5,418件の閲覧回数
liyigang
Contributor III

hi,

     On imx6 platform, use yocto warrior to generate Wayland image, QT program or chromium can be run manually at the terminal,However, there is no response to the automatic running of QT program at boot time。

   Wayland doesn't seem to have the. Desktop function. What do I need to do if I want to run an X application automatically?

ラベル(4)
1 解決策
5,351件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Li yigang,

The question is not related to i.MX or linux BSP, just on how to run a application automatically when linux starts up.

Actually , you can get a lot of experience from internet.

for you question, it is very similar to boot on ubuntu :

-------------------------

Open/home/root/.profile, and the line:

/usr/bin/chromium/chrome --no-sandbox --disable-setuid-sandbox --user-data-dir=/home/root

------------------------

Try it, please!

Have  a nice day!

B.R,

weidong

元の投稿で解決策を見る

4 返答(返信)
5,351件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

  X application should run on the xwayland image, not wayland.

Hope the information is helpful to you.

Have a nice day!

B.R,

Weidong

0 件の賞賛
返信
5,351件の閲覧回数
liyigang
Contributor III

The following two ways of making images have been tried

DISTRO=fsl-imx-xwayland MACHINE=imx6qsabresd source fsl-setup-release.sh -b build-xwayland

DISTRO=fsl-imx-wayland MACHINE=imx6qsabresd source fsl-setup-release.sh -b build-wayland

I want to run chromium automatically when I starting up

0 件の賞賛
返信
5,352件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Li yigang,

The question is not related to i.MX or linux BSP, just on how to run a application automatically when linux starts up.

Actually , you can get a lot of experience from internet.

for you question, it is very similar to boot on ubuntu :

-------------------------

Open/home/root/.profile, and the line:

/usr/bin/chromium/chrome --no-sandbox --disable-setuid-sandbox --user-data-dir=/home/root

------------------------

Try it, please!

Have  a nice day!

B.R,

weidong

5,351件の閲覧回数
liyigang
Contributor III

thank you

0 件の賞賛
返信