IMX6SOLOX processor maximium supported density for NOR Flash IC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6SOLOX processor maximium supported density for NOR Flash IC

1,650 Views
deepa_sharma071
Contributor I

 what is the maximium density supported by IMX6SOLOX processor for NOR flash IC ? 

Labels (1)
0 Kudos
Reply
1 Reply

1,557 Views
radhikasomaiya
Senior Contributor II

Hi Deepa Sharma,

You can refer the imx6solox reference manual section 2.2 which provides the chip memory details along with its depth and range. For NOR flash with EIM interface the depth is 128 MB and for NOR flash with QSPI has the depth of  256 MB.

i.MX 6SoloX Applications Processor Reference Manual

Regards,

Radhika