How to run the sdk_unit_test ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to run the sdk_unit_test ?

跳至解决方案
1,651 次查看
patcharasirigul
Contributor II

Hello everyone,

     I downloaded the i.MX 6Series Platform SDK. I'd like to know how to run all_test.c or unit_test_main.c for testing the SABRE-SD Board.

Thank you,

标签 (3)
0 项奖励
回复
1 解答
1,561 次查看
saurabh206
Senior Contributor III

Hi,

You can refer iMX6_Platform_SDK\doc

Which provides all the information.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,561 次查看
Yuri
NXP Employee
NXP Employee

  Please take a look at README.pdf file in the SDK package.

Also, to build the tests, Linux host is preferable.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,562 次查看
saurabh206
Senior Contributor III

Hi,

You can refer iMX6_Platform_SDK\doc

Which provides all the information.

0 项奖励
回复