How to run the sdk_unit_test ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to run the sdk_unit_test ?

Jump to solution
1,654 Views
patcharasirigul
Contributor II

Hello everyone,

     I downloaded the i.MX 6Series Platform SDK. I'd like to know how to run all_test.c or unit_test_main.c for testing the SABRE-SD Board.

Thank you,

Labels (3)
0 Kudos
Reply
1 Solution
1,564 Views
saurabh206
Senior Contributor III

Hi,

You can refer iMX6_Platform_SDK\doc

Which provides all the information.

View solution in original post

0 Kudos
Reply
2 Replies
1,564 Views
Yuri
NXP Employee
NXP Employee

  Please take a look at README.pdf file in the SDK package.

Also, to build the tests, Linux host is preferable.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,565 Views
saurabh206
Senior Contributor III

Hi,

You can refer iMX6_Platform_SDK\doc

Which provides all the information.

0 Kudos
Reply