How to reduce the brightness of the OLED(MIPI) display

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to reduce the brightness of the OLED(MIPI) display

10,157 次查看
nandishguruling
Contributor III

Hello ALL,

    i am using the OLED display (DLC0139AZOG-1) with imx6DL board,  i want to reduce the brightness of this display,

   for this i need to control the  SWIRE Pin which has address of ( 0x2Ah for mipi address) and i wrote in driver which is not

   change anything on display, please  any one can see the below code and tell me what wrong i did in the code,

   in the below code in macros is i changed some vaues i commented like //Brightness Related Start & End after changing

   those values while booting time display brightnes is less after complete the booting the display brightness is high,


#include <linux/types.h>
#include <linux/init.h>
#include <linux/delay.h>
#include <linux/platform_device.h>
#include <linux/err.h>
#include <linux/clk.h>
#include <linux/console.h>
#include <linux/io.h>
#include <linux/bitops.h>
#include <linux/spinlock.h>
#include <linux/mipi_dsi.h>
#include <linux/mxcfb.h>
#include <linux/backlight.h>
#include <video/mipi_display.h>

#include "mipi_dsi.h"

#define MIPI_DSI_MAX_RET_PACK_SIZE                (0x4)
//it was 255 on both max and def
#define HX8369BL_MAX_BRIGHT        (255)
#define HX8369BL_DEF_BRIGHT        (128)

#define HX8369_MAX_DPHY_CLK                    (800)
#define HX8369_ONE_DATA_LANE                    (0x1)
#define HX8369_TWO_DATA_LANE                    (0x2)

#define HX8369_CMD_SETEXTC                    (0xB9)
#define HX8369_CMD_SETEXTC_LEN                    (0x4)
#define HX8369_CMD_SETEXTC_PARAM_1                (0x6983ff)

#define HX8369_CMD_GETHXID                    (0xF4)
#define HX8369_CMD_GETHXID_LEN                    (0x4)
#define HX8369_ID                        (0x69)
#define HX8369_ID_MASK                        (0xFF)

#define HX8369_CMD_SETDISP                    (0xB2)
#define HX8369_CMD_SETDISP_LEN                    (16)
#define HX8369_CMD_SETDISP_1_HALT                (0x00)
#define HX8369_CMD_SETDISP_2_RES_MODE                (0x23)
#define HX8369_CMD_SETDISP_3_BP                    (0x03)
#define HX8369_CMD_SETDISP_4_FP                    (0x03)
#define HX8369_CMD_SETDISP_5_SAP                (0x70)
#define HX8369_CMD_SETDISP_6_GENON                (0x00)
#define HX8369_CMD_SETDISP_7_GENOFF                (0xff)
#define HX8369_CMD_SETDISP_8_RTN                (0x00)
#define HX8369_CMD_SETDISP_9_TEI                (0x00)
#define HX8369_CMD_SETDISP_10_TEP_UP                (0x00)
#define HX8369_CMD_SETDISP_11_TEP_LOW                (0x00)
#define HX8369_CMD_SETDISP_12_BP_PE                (0x03)
#define HX8369_CMD_SETDISP_13_FP_PE                (0x03)
#define HX8369_CMD_SETDISP_14_RTN_PE                (0x00)
#define HX8369_CMD_SETDISP_15_GON                (0x01)

#define HX8369_CMD_SETCYC                    (0xB4)
#define HX8369_CMD_SETCYC_LEN                    (6)
#define HX8369_CMD_SETCYC_PARAM_1                (0x5f1d00)
#define HX8369_CMD_SETCYC_PARAM_2                (0x060e)

#define HX8369_CMD_SETGIP                    (0xD5)
#define HX8369_CMD_SETGIP_LEN                    (27)
#define HX8369_CMD_SETGIP_PARAM_1                (0x030400)
#define HX8369_CMD_SETGIP_PARAM_2                (0x1c050100)
#define HX8369_CMD_SETGIP_PARAM_3                (0x00030170)
#define HX8369_CMD_SETGIP_PARAM_4                (0x51064000)
#define HX8369_CMD_SETGIP_PARAM_5                (0x41000007)
#define HX8369_CMD_SETGIP_PARAM_6                (0x07075006)
#define HX8369_CMD_SETGIP_PARAM_7                (0x040f)

#define HX8369_CMD_SETPOWER                    (0xB1)
#define HX8369_CMD_SETPOWER_LEN                    (20)
#define HX8369_CMD_SETPOWER_PARAM_1                (0x340001)
#define HX8369_CMD_SETPOWER_PARAM_2                (0x0f0f0006)
#define HX8369_CMD_SETPOWER_PARAM_3                (0x3f3f322a)
#define HX8369_CMD_SETPOWER_PARAM_4                (0xe6013a07)
#define HX8369_CMD_SETPOWER_PARAM_5                (0xe6e6e6e6)

#define HX8369_CMD_SETVCOM                    (0xB6)
#define HX8369_CMD_SETVCOM_LEN                    (3)
#define HX8369_CMD_SETVCOM_PARAM_1                (0x5656)

#define HX8369_CMD_SETPANEL                    (0xCC)
#define HX8369_CMD_SETPANEL_PARAM_1                (0x02)

#define HX8369_CMD_SETGAMMA                    (0xE0)
#define HX8369_CMD_SETGAMMA_LEN                    (35)
#define HX8369_CMD_SETGAMMA_PARAM_1                (0x221d00)
#define HX8369_CMD_SETGAMMA_PARAM_2                (0x2e3f3d38)
#define HX8369_CMD_SETGAMMA_PARAM_3                (0x0f0d064a)
#define HX8369_CMD_SETGAMMA_PARAM_4                (0x16131513)
#define HX8369_CMD_SETGAMMA_PARAM_5                (0x1d001910)
#define HX8369_CMD_SETGAMMA_PARAM_6                (0x3f3d3822)
#define HX8369_CMD_SETGAMMA_PARAM_7                (0x0d064a2e)
#define HX8369_CMD_SETGAMMA_PARAM_8                (0x1315130f)
#define HX8369_CMD_SETGAMMA_PARAM_9                (0x191016)

#define HX8369_CMD_SETMIPI                    (0xBA)
#define HX8369_CMD_SETMIPI_LEN                    (14)
#define HX8369_CMD_SETMIPI_PARAM_1                (0xc6a000)
#define HX8369_CMD_SETMIPI_PARAM_2                (0x10000a00)
#define HX8369_CMD_SETMIPI_ONELANE                (0x10 << 24)
#define HX8369_CMD_SETMIPI_TWOLANE                (0x11 << 24)
#define HX8369_CMD_SETMIPI_PARAM_3                (0x00026f30)
#define HX8369_CMD_SETMIPI_PARAM_4                (0x4018)

#define HX8369_CMD_SETPIXEL_FMT                    (0x3A)
#define HX8369_CMD_SETPIXEL_FMT_24BPP                (0x77)
#define HX8369_CMD_SETPIXEL_FMT_18BPP                (0x66)
#define HX8369_CMD_SETPIXEL_FMT_16BPP                (0x55)

#define HX8369_CMD_SETCLUMN_ADDR                (0x2A)
#define HX8369_CMD_SETCLUMN_ADDR_LEN                (5)
#define HX8369_CMD_SETCLUMN_ADDR_PARAM_1            (0xdf0000)
#define HX8369_CMD_SETCLUMN_ADDR_PARAM_2            (0x01)

#define HX8369_CMD_SETPAGE_ADDR                    (0x2B)
#define HX8369_CMD_SETPAGE_ADDR_LEN                (5)
#define HX8369_CMD_SETPAGE_ADDR_PARAM_1                (0x1f0000)
#define HX8369_CMD_SETPAGE_ADDR_PARAM_2                (0x03)

//Brightness Related  Start
#define HX8369_CMD_WRT_DISP_BRIGHT                (0x51)
#define HX8369_CMD_WRT_DISP_BRIGHT_PARAM_1            (0x80)
//FF up it was
#define HX8369_CMD_WRT_CABC_MIN_BRIGHT                (0x5E)
#define HX8369_CMD_WRT_CABC_MIN_BRIGHT_PARAM_1            (0x10)
//20 up it was
#define HX8369_CMD_WRT_CABC_CTRL                (0x55)
#define HX8369_CMD_WRT_CABC_CTRL_PARAM_1            (0x0)
//1 up it was
#define HX8369_CMD_WRT_CTRL_DISP                (0x53)
#define HX8369_CMD_WRT_CTRL_DISP_PARAM_1            (0x24)

//Brightness Related End
#define CHECK_RETCODE(ret)                    \
do {                                \
    if (ret < 0) {                        \
        dev_err(&mipi_dsi->pdev->dev,            \
            "%s ERR: ret:%d, line:%d.\n",        \
            __func__, ret, __LINE__);        \
        return ret;                    \
    }                            \
} while (0)

static int hx8369bl_brightness;
static int mipid_init_backlight(struct mipi_dsi_info *mipi_dsi);

static struct fb_videomode truly_lcd_modedb[] = {
    {
     "TRULY-WVGA", 60, 400, 400, 69643,
     40, 20,
     12, 20,
     20, 4,
     FB_SYNC_OE_LOW_ACT,
     FB_VMODE_NONINTERLACED,
     0,
    },
};

static struct mipi_lcd_config lcd_config = {
    .virtual_ch    = 0,
    .data_lane_num  = 1,
    .max_phy_clk    = 350,
    .dpi_fmt    = MIPI_RGB888,
};
void mipid_hx8369_get_lcd_videomode(struct fb_videomode **mode, int *size,
        struct mipi_lcd_config **data)
{       
        printk(" MIPI DRIVER IS READY\n\n\n\n");
    *mode = &truly_lcd_modedb[0];
    *size = ARRAY_SIZE(truly_lcd_modedb);
    *data = &lcd_config;
}

int mipid_hx8369_lcd_setup(struct mipi_dsi_info *mipi_dsi)
{
    u32 buf[DSI_CMD_BUF_MAXSIZE];
    int err;
        printk(" MIPI LCD SETUP IS CALLED\n\n\n\n");

    buf[0] = MIPI_DSI_MAX_RET_PACK_SIZE;
    err = mipi_dsi_pkt_write(mipi_dsi,
                MIPI_DSI_SET_MAXIMUM_RETURN_PACKET_SIZE,
                buf, 0);
    CHECK_RETCODE(err);

//SWIRE ADDRESS
        buf[0] = 0x2A;
    err = mipi_dsi_pkt_write(mipi_dsi, MIPI_DSI_GENERIC_SHORT_WRITE_2_PARAM,
        buf, 0);
    CHECK_RETCODE(err);


    /* Set power: standby, DC etc. */
    buf[0] = HX8369_CMD_SETPOWER | (HX8369_CMD_SETPOWER_PARAM_1 << 8);
    buf[1] = HX8369_CMD_SETPOWER_PARAM_2;
    buf[2] = HX8369_CMD_SETPOWER_PARAM_3;
    buf[3] = HX8369_CMD_SETPOWER_PARAM_4;
    buf[4] = HX8369_CMD_SETPOWER_PARAM_5;
    err = mipi_dsi_pkt_write(mipi_dsi, MIPI_DSI_GENERIC_LONG_WRITE, buf,
                HX8369_CMD_SETPOWER_LEN);
    CHECK_RETCODE(err);


/* Set display brightness related */
    buf[0] = HX8369_CMD_WRT_DISP_BRIGHT |
            (HX8369_CMD_WRT_DISP_BRIGHT_PARAM_1 << 8);
    err = mipi_dsi_pkt_write(mipi_dsi, MIPI_DSI_GENERIC_SHORT_WRITE_2_PARAM,
        buf, 0);
    CHECK_RETCODE(err);                                                                            

    buf[0] = HX8369_CMD_WRT_CABC_CTRL |
        (HX8369_CMD_WRT_CABC_CTRL_PARAM_1 << 8);
    err = mipi_dsi_pkt_write(mipi_dsi, MIPI_DSI_GENERIC_SHORT_WRITE_2_PARAM,
        buf, 0);
    CHECK_RETCODE(err);

    buf[0] = HX8369_CMD_WRT_CTRL_DISP |
        (HX8369_CMD_WRT_CTRL_DISP_PARAM_1 << 8);
    err = mipi_dsi_pkt_write(mipi_dsi, MIPI_DSI_GENERIC_SHORT_WRITE_2_PARAM,
        buf, 0);
    CHECK_RETCODE(err);

    /* exit sleep mode and set display on */
    buf[0] = MIPI_DCS_EXIT_SLEEP_MODE;
    err = mipi_dsi_pkt_write(mipi_dsi, MIPI_DSI_GENERIC_SHORT_WRITE_1_PARAM,
        buf, 0);
    CHECK_RETCODE(err);
    /* To allow time for the supply voltages
     * and clock circuits to stabilize.
     */
    msleep(5);
    buf[0] = MIPI_DCS_SET_DISPLAY_ON;
    err = mipi_dsi_pkt_write(mipi_dsi, MIPI_DSI_GENERIC_SHORT_WRITE_1_PARAM,
        buf, 0);
    CHECK_RETCODE(err);

    err = mipid_init_backlight(mipi_dsi);
    return err;
}

static int mipid_bl_update_status(struct backlight_device *bl)
{
    u32 buf;
    int brightness = bl->props.brightness;
        printk(" MIPI LCD BL UPDATE STATUS:\n\n\n\n");
    struct mipi_dsi_info *mipi_dsi = bl_get_data(bl);

    if (bl->props.power != FB_BLANK_UNBLANK ||
        bl->props.fb_blank != FB_BLANK_UNBLANK)
        brightness = 0;

    buf = HX8369_CMD_WRT_DISP_BRIGHT |
            ((brightness & HX8369BL_MAX_BRIGHT) << 8);
    mipi_dsi_pkt_write(mipi_dsi, MIPI_DSI_GENERIC_SHORT_WRITE_2_PARAM,
        &buf, 0);

    hx8369bl_brightness = brightness & HX8369BL_MAX_BRIGHT;

    dev_dbg(&bl->dev, "mipid backlight bringtness:%d.\n", brightness);
    return 0;
}

static int mipid_bl_get_brightness(struct backlight_device *bl)
{
    return hx8369bl_brightness;
}

static int mipi_bl_check_fb(struct backlight_device *bl, struct fb_info *fbi)
{
    return 0;
}

static const struct backlight_ops mipid_lcd_bl_ops = {
    .update_status = mipid_bl_update_status,
    .get_brightness = mipid_bl_get_brightness,
    .check_fb = mipi_bl_check_fb,
};

static int mipid_init_backlight(struct mipi_dsi_info *mipi_dsi)
{
        
    struct backlight_properties props;
    struct backlight_device    *bl;
        
    if (mipi_dsi->bl) {
        pr_debug("mipid backlight already init!\n");
        return 0;
    }
        printk(" MIPI LCD INIT BACKLIGHT\n\n\n\n");//nand
    memset(&props, 0, sizeof(struct backlight_properties));
    props.max_brightness = HX8369BL_MAX_BRIGHT;
    props.type = BACKLIGHT_RAW;
    bl = backlight_device_register("mipid-bl", &mipi_dsi->pdev->dev,
        mipi_dsi, &mipid_lcd_bl_ops, &props);
    if (IS_ERR(bl)) {
        pr_err("error %ld on backlight register\n", PTR_ERR(bl));
        return PTR_ERR(bl);
    }
    mipi_dsi->bl = bl;
    bl->props.power = FB_BLANK_UNBLANK;
    bl->props.fb_blank = FB_BLANK_UNBLANK;
    bl->props.brightness = HX8369BL_DEF_BRIGHT;

    mipid_bl_update_status(bl);
    return 0;
}

Thanks in advance

best regards

nandish sg

0 项奖励
回复
11 回复数

9,045 次查看
nandishguruling
Contributor III

Hi Daniel,

You can control the brightness of MIPI Display from user space by giving the commands for brightness,

in terminal   "echo 255 > /sys/class/backlight/mipid-bl/brightness" , (0 to 255 is brightness value), 

Best Regards

Nandish SG

0 项奖励
回复

9,044 次查看
nandishguruling
Contributor III

Hi All,

      I resolved the Issue of Brightness Control of MIPI Display and Thanks to Igor for Helping in this issue.

Best Regards

Nandish SG    

0 项奖励
回复

9,045 次查看
danielgarbanzoh
Contributor I

Hi Nandish,

Could you please tell me how do you resolve the Brightness Control of MIPI Display issue? Did you use a different approach from the mentioned above? 

I am trying to expose Brightness Control of MIPI Display from user_space, so you issue fix may help me a lot.

Thanks in advance!

Best regards,

-Daniel 

0 项奖励
回复

9,045 次查看
nandishguruling
Contributor III

Hi Igor,

can you please have a look for reading the brightness in terminal, when i give the 128 in brightness it shows the voltage as 3.3v,

root@imx6dlsabreauto:/sys/class/backlight/mipid-bl# cat brightness
50
root@imx6dlsabreauto:/sys/class/backlight/mipid-bl# echo 128 > brightness
WHAT BRIGHTNESS I GET = 128

 MIPI LCD BL UPDATE STATUS:

 MIPI LCD BL FB_BLANK_UNBLANK= 0

NOW BRIGHTNESS I GET = 128

mipi_dsi_pkt_write BUF = 32810

MIPI_DSI_CMD_PKT_STATUS val = 0x1515

root@imx6dlsabreauto:/sys/class/backlight/mipid-bl# cat brightness
128
root@imx6dlsabreauto:/sys/class/backlight/mipid-bl# cat actual_brightness
128
root@imx6dlsabreauto:/sys/class/backlight/mipid-bl# cat max_brightness
128
root@imx6dlsabreauto:/sys/class/backlight/mipid-bl#

when change it to 64 in brightness value it shows the voltage as again 3.3v. i am expecting the low voltage(whether i am correct or wrong please tell me),

root@imx6dlsabreauto:/sys/class/backlight/mipid-bl# echo 64 > brightness
WHAT BRIGHTNESS I GET = 64

MIPI LCD BL UPDATE STATUS:

MIPI LCD BL FB_BLANK_UNBLANK= 0

NOW BRIGHTNESS I GET = 64

mipi_dsi_pkt_write BUF = 42

MIPI_DSI_CMD_PKT_STATUS val = 0x1515

root@imx6dlsabreauto:/sys/class/backlight/mipid-bl# cat actual_brightness
0
root@imx6dlsabreauto:/sys/class/backlight/mipid-bl# cat brightness
64
root@imx6dlsabreauto:/sys/class/backlight/mipid-bl# cat max_brightness
128
root@imx6dlsabreauto:/sys/class/backlight/mipid-bl#

can any one please suggest me where i am wrong,

thanks in advance

best regards

Nandish sg

0 项奖励
回复

9,045 次查看
nandishguruling
Contributor III

Hi igor,

yes i check with the DLC Datasheet they are mentioned in datasheet  this value

pastedImage_1.png

in Application notes they mentioned that

(2A80h) SWIRE Control

(8F80h) DIMCTR

(9080h) DIMCTRDP1

(9180h) DIMCTRDP2

(9280h) DIMCTRDP3

i tried all the above values in place of " HX8369_CMD_WRT_DISP_BRIGHT"

 /* Set display brightness related */
    buf[0] = HX8369_CMD_WRT_DISP_BRIGHT |
            (HX8369_CMD_WRT_DISP_BRIGHT_PARAM_1 << 8);
    err = mipi_dsi->mipi_dsi_pkt_write(mipi_dsi, MIPI_DSI_GENERIC_SHORT_WRITE_2_PARAM,
        buf, 0);
    CHECK_RETCODE(err);

but i am not seen any change in the display

Thanks in advance

BR

nandish sg

0 项奖励
回复

9,045 次查看
igorpadykov
NXP Employee
NXP Employee

Hi nandish

 

one can check real brightness reading it back.

 

Best regards
igor

0 项奖励
回复

9,045 次查看
nandishguruling
Contributor III

Hi igor,

Thanks for your reply, i set the HX8369_CMD_WRT_DISP_BRIGHT_PARAM_1 = 0xFF is default value and  i changed to 0x80, no change in display,  you can see the my first mail on top i added 2 pics while boot time brightness is low after booting brightness is high,

thanks in advance

BR

nandish sg

0 项奖励
回复

9,045 次查看
igorpadykov
NXP Employee
NXP Employee

Hi nandish

one can check OLED display DLC0139AZOG datasheet

for brightness commands.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

9,045 次查看
nandishguruling
Contributor III

Hi igor,

Thank you for your feedback, i am using the same driver what you mentioned in the above reply, 

git/drivers/video/mxc/mxcfb_hx8363_wvga.c , but no change in display,

Thanks in advance

BR

nandish  sg

0 项奖励
回复

9,045 次查看
igorpadykov
NXP Employee
NXP Employee

Hi nandish

 

there is example in mxcfb_hx8369_wvga.c function mipid_hx8369_lcd_setup() :

    /* Set display brightness related */
    buf[0] = HX8369_CMD_WRT_DISP_BRIGHT |
            (HX8369_CMD_WRT_DISP_BRIGHT_PARAM_1 << 8);
    err = mipi_dsi->mipi_dsi_pkt_write(mipi_dsi, MIPI_DSI_GENERIC_SHORT_WRITE_2_PARAM,
        buf, 0);
    CHECK_RETCODE(err); ..

Best regards
igor

0 项奖励
回复

9,045 次查看
igorpadykov
NXP Employee
NXP Employee

Hi nandish

please look at brightness example on
linux/drivers/video/fbdev/mxc/mxcfb_hx8363_wvga.c

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复