How to reduce power consumption in deep sleep mode in imx6dl?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to reduce power consumption in deep sleep mode in imx6dl?

6,691件の閲覧回数
nayan_khant
Contributor I

Hi All,

One customised board based on iMX.6DL processor, consume around 200mW power in deep sleep mode with Linux OS, is this admissible?

And also observe that PMIC (pf0100) does not get into STANDBY or SLEEP mode.

Please help me here, to optimize power consumption during sleep mode.

Thanks,

Nayan Khant

ラベル(2)
0 件の賞賛
返信
7 返答(返信)

6,241件の閲覧回数
alice434
Contributor I

For any kind of technical related query regarding Apple or its operating system, then contact Apple technical service for the best solution. Hope this will help you.

                                                     

0 件の賞賛
返信

6,241件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nayan

one can check suggestions provided in sect.4 Reducing power consumption AN4576

i.MX 6DualLite Power Consumption Measurement 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

6,241件の閲覧回数
nayan_khant
Contributor I

Thanks, igor for a quick response.

In i.MX 6DualLite Power Consumption Measurement document section 3.2.1 mentioned that in deep sleep mode VDDARM_IN & VDDSOC_IN should be drop to 0.9 volts (this should be done by PMIC).

But in my case, it remains as same 1.375 volts.

Any thoughts?

0 件の賞賛
返信

6,241件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

reason may be that your is not based on i.MX6DL NXP Sabre SD design spf-27392

schematic available on

Schematics (1)
Design files, including hardware schematics, Gerbers, and OrCAD files.
SABRE Platform for Smart Devices | NXP 

and not used nxp official bsp from nxp repository

linux-imx - i.MX Linux kernel 

One can try with i.MX6DL Sabre SD board and Demo Images from

i.MX Software | NXP 

Best regards
igor

6,239件の閲覧回数
mrudangshelat1
Senior Contributor II

Hi Igor,

I have checked the schematic against the i.MX6DL NXP Sabre SD design spf-27392, but I don't find major changes in the circuit. I have attached our schematic for your reference. Please check and let me know what are the other changes required to reduce the power of our device.

Thanks,

Mrudang

0 件の賞賛
返信

6,239件の閲覧回数
mrudangshelat1
Senior Contributor II

HI,

Any updates here?

Regards,

Mrudang

0 件の賞賛
返信

6,239件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Mrudang

one can test with i.MX6DL NXP Sabre SD design spf-27392

using Demo Images from

i.MX Software | NXP 

May be useful to check app notes:

Measuring Current in i.MX Applications

i.MX 6DualLite Power Consumption Measurement

For custom board optimizations may be recommended to use extended support with

NXP Professional Services | NXP 

Best regards
igor

0 件の賞賛
返信