How to program i.MX8M Mini eFUSE during First Load?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to program i.MX8M Mini eFUSE during First Load?

Jump to solution
2,007 Views
lumen
Contributor III

Hi,

We are designing a custom board with the i.MX8M Mini, SPI Flash and eMMC. If neither the processor nor the flashes are programmed, is it possible to burn the eFuses during the first load (e.x. with JTAG)?

The plan is to do the following steps during manufacturing and testing of the board:

1. Programm SPI Flash with Rescue Image over Needleadapter

2. Burn eFuses from i.MX8M Mini to boot from SPI Flash

3. Start i.MX8M Mini from SPI Flash

Is the described first load according the steps above possible?

Best Regards,

Patrick

0 Kudos
Reply
1 Solution
2,003 Views
Yuri
NXP Employee
NXP Employee

@lumen 
Hello,

  the recommended ways to burn the fuses are described in the following
tutorial:

https://imxdev.gitlab.io/tutorial/Burning_eFuses_on_i.MX8_and_i.MX8x_families/

https://imxdev.gitlab.io/tutorial/How_to_use_UUU_to_flash_the_iMX_boards/

 Note: UUU allows to program the fuses, using internal i.MX serial downloader,
without any boot images on the board.

Regards,
Yuri.

View solution in original post

0 Kudos
Reply
1 Reply
2,004 Views
Yuri
NXP Employee
NXP Employee

@lumen 
Hello,

  the recommended ways to burn the fuses are described in the following
tutorial:

https://imxdev.gitlab.io/tutorial/Burning_eFuses_on_i.MX8_and_i.MX8x_families/

https://imxdev.gitlab.io/tutorial/How_to_use_UUU_to_flash_the_iMX_boards/

 Note: UUU allows to program the fuses, using internal i.MX serial downloader,
without any boot images on the board.

Regards,
Yuri.

0 Kudos
Reply