How to program i.MX8M Mini eFUSE during First Load?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to program i.MX8M Mini eFUSE during First Load?

ソリューションへジャンプ
1,954件の閲覧回数
lumen
Contributor III

Hi,

We are designing a custom board with the i.MX8M Mini, SPI Flash and eMMC. If neither the processor nor the flashes are programmed, is it possible to burn the eFuses during the first load (e.x. with JTAG)?

The plan is to do the following steps during manufacturing and testing of the board:

1. Programm SPI Flash with Rescue Image over Needleadapter

2. Burn eFuses from i.MX8M Mini to boot from SPI Flash

3. Start i.MX8M Mini from SPI Flash

Is the described first load according the steps above possible?

Best Regards,

Patrick

0 件の賞賛
返信
1 解決策
1,950件の閲覧回数
Yuri
NXP Employee
NXP Employee

@lumen 
Hello,

  the recommended ways to burn the fuses are described in the following
tutorial:

https://imxdev.gitlab.io/tutorial/Burning_eFuses_on_i.MX8_and_i.MX8x_families/

https://imxdev.gitlab.io/tutorial/How_to_use_UUU_to_flash_the_iMX_boards/

 Note: UUU allows to program the fuses, using internal i.MX serial downloader,
without any boot images on the board.

Regards,
Yuri.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,951件の閲覧回数
Yuri
NXP Employee
NXP Employee

@lumen 
Hello,

  the recommended ways to burn the fuses are described in the following
tutorial:

https://imxdev.gitlab.io/tutorial/Burning_eFuses_on_i.MX8_and_i.MX8x_families/

https://imxdev.gitlab.io/tutorial/How_to_use_UUU_to_flash_the_iMX_boards/

 Note: UUU allows to program the fuses, using internal i.MX serial downloader,
without any boot images on the board.

Regards,
Yuri.

0 件の賞賛
返信