How to power up iMX6UL without a button

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to power up iMX6UL without a button

1,223 次查看
alcon
Contributor I

I would like to connect the ONOFF pin so the CPU will power-up when applying power to the board, without a button.

Can I just connect it to GND? I'm afraid the the CPU will power off after few seconds (simulating a long button press).

Thanks.

标签 (1)
0 项奖励
回复
2 回复数

1,137 次查看
b36401
NXP Employee
NXP Employee

In common words the board simply should meet the power up sequence.
So if power up sequence is OK it is no matter if the board is started turning on the switch or directly with connecting the power.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,137 次查看
alcon
Contributor I

Thanks for your answer.

So if I understand correctly - there is no need to deassert the ONOFF pin in order to power up the CPU. Is it correct? 

0 项奖励
回复