How to power up iMX6UL without a button

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to power up iMX6UL without a button

1,222 Views
alcon
Contributor I

I would like to connect the ONOFF pin so the CPU will power-up when applying power to the board, without a button.

Can I just connect it to GND? I'm afraid the the CPU will power off after few seconds (simulating a long button press).

Thanks.

Labels (1)
0 Kudos
Reply
2 Replies

1,136 Views
b36401
NXP Employee
NXP Employee

In common words the board simply should meet the power up sequence.
So if power up sequence is OK it is no matter if the board is started turning on the switch or directly with connecting the power.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,136 Views
alcon
Contributor I

Thanks for your answer.

So if I understand correctly - there is no need to deassert the ONOFF pin in order to power up the CPU. Is it correct? 

0 Kudos
Reply