How to perform tftp boot in i.MX8M Plus ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to perform tftp boot in i.MX8M Plus ?

1,788 Views
Jimmychea
Contributor III

May i know how to perform tftp boot in i.MX8M Plus LPDDR4 EVK? Thanks

0 Kudos
Reply
1 Reply

1,766 Views
Dhruvit
NXP TechSupport
NXP TechSupport

Hi @Jimmychea,

I hope you are doing well.

One needs to Install and configure a TFTP server on a host computer that is connected to the same network as the i.MX8MPlus LPDDR EVK and copy the required kernel Image and dtb to TFTP_DIRECTORY.
 
Then write the bootloader (imx-boot*) image to emmc/sd using the below command.
uuu -b emmc bootloader
 
Power on the board and stop at the uboot cmd line. and run below mentioned commands.
 
For further steps, one can refer to 4.4.1.2 Downloading an image to MMC/SD in i.MX Linux User's Guide
 
Thanks & Regards,
Dhruvit Vasavada.
0 Kudos
Reply