How to output 25 MHz Clock from RGMII_TXC pin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to output 25 MHz Clock from RGMII_TXC pin

3,649 Views
mehmetipin
Contributor II

Dear Community,

I have i.mx6dl based board with Micrel KSZ9021 PHY.  PHY needs 25 MHz clock from MX6 MAC to generate 125 MHz reference clock, in its RGMII mode. 

I am using u-boot 2009.08.  There is 6 MHz clock at RGMII_TXC pin. Is it possible to output 25 MHz clock from this pin?  If yes, How can I do it?

Thanks and best regards.

Mehmet Ali Ipin

Labels (2)
8 Replies

3,068 Views
mehmetipin
Contributor II

Dear Gusarambula,

Thank you for your pations and informations; Unfortunately I don't have GPIO_16 pin to generate 125MHz clock.  

I know MAC needs 125 MHZ clock from PHY/or external source. PHY(9021) also needs 25 MHz clock in its GTX_CLK pin to generate 125 MHz ENET_REF_CLK. My PHY schematic is same as MCIMX6QP-SDB. I connected RGMII_TXC to GTX_CLK and RGMII_TX_CTL pin TX_EN pin of PHY.

In fact I Have 6 MHz at RGMII_TXC pin, and PHY is generating 30 MHz(5*GTX_CLK) (if it was 25, PHY will generate 125MHz) to ENET_REF_CLK pin of MX6.

I only need informations, what should I do to generate 25 MHz clock instead of 6 MHz from RGMII_TXC pin?

 
 
 
 
0 Kudos
Reply

3,068 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Mehmet Ali Ipin,

I'm currently double checking if it's possible to generate the 25Mhz clock from RGMII_TXC as your design requires. I'll update this thread as soon as I have more information.

Regards,

3,068 Views
MehmetAliIpin
Contributor V

Dear Gusarambula,

Thank you very much for your interests.

Thanks and best regards.

0 Kudos
Reply

3,068 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Mehmet Ali Ipin,

My apologies. I double checked and confirmed that it’s not possible to multiplex RGMII_TXC as 25MHz reference clock output for RGMII PHY.

i.MX6Q can output a 50MHz reference clock from GPIO_16 or RGMII_TX_CTL for RMII application. If GPIO_16 is available, it might be able to output a 25MHz clock for the RGMII PHY.

In your case since GPIO_16 is not available the best alternative would be adding a 25MHz crystal on the PHY since the RGMII_TXC pin cannot generate it.

Regards,

0 Kudos
Reply

3,068 Views
MehmetAliIpin
Contributor V

Dear Gusarambula,

Thank you for your informations.

Best regards.

0 Kudos
Reply

3,068 Views
MehmetAliIpin
Contributor V

Dear Gusarambula,

Thank you very much for your informations.

I read section 10.4.2 of Hardware guide. It explains RGMII_TX_CTL pin to generate the reference clock, and there is nothing with RGMII_TXC pin.  I am very confused;

  • Are we using RGMII_TX_CTL pin in order to output clock signal from RGMII_TXC pin?
  • Is it possible to generate 25 MHz clock at the RGMII_TXC pin?
  • What is the reference of RGMII_TXC clock CCM_ANALOG_PLL_ENETn  or external 125 MHz?

Best regards.

Mehmet

0 Kudos
Reply

3,068 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Mehmet,

My apologies for not being clear. I believe your scenario is similar to the one described on the following thread:

https://community.nxp.com/message/539982

If you wish to generate the PHY clock on the i.MX6 you may do so but you should use either GPIO_16 or RGMII_TX_CTL as output; and then input the 125MHZ from the PHY to ENET_REF_CLK.

The reason being that the RGMII_TXC pin is generated from the ENET module but the module itself requires the 125Mhz clock for RGMII. RGMII_TXC should thus be used as signal for the RGMII but not as reference clock.

Pins GPIO_16 or RGMII_TX_CTL may be used to generate the clock from the PLLs and then provide to the PHY. These pins would be controlled with register CCM_ANALOG_PLL_ENETn.

I hope this information helps!

Regards,

0 Kudos
Reply

3,068 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Mehmet Ali Ipin,

You can find information on how to achieve this in section 10.4.2 of the i.MX6 Hardware Guide (link below).

http://www.nxp.com/assets/documents/data/en/user-guides/IMX6DQ6SDLHDG.pdf

Please also look at bits CCM_ANALOG_PLL_ENETn[0:1], as listed on section 18.7.15 of the i.MX6Q Reference Manual.

I hope this information helps!

Regards,

0 Kudos
Reply